TE Connectivity L000659-02 Tri-Band Antenna, Now at Mouser, Enables Wi-Fi 6E/7 Connectivity
June 12, 2024 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the L000659-02 Wi-Fi® 6E Tri-Band antenna from TE Connectivity.
TE Connectivity's L000659-02 Wi-Fi 6E Tri-Band antenna is a 2.4GHz to 2.5GHz, 4.9GHz to 6GHz, and 6GHz to 7.125GHz center-fed omnidirectional array antenna. This antenna is specifically designed to complement interior or exterior-mounted Wi-Fi 6E wireless network systems. The L000659-02 antenna comes equipped with an integrated and rotatable type-N male connector and a sleeved base, facilitating easy installation. This omnidirectional array antenna offers a high-performance beam pattern and tri-band Wi-Fi coverage, including legacy Wi-Fi, Wi-Fi 6, Wi-Fi 6E, and Wi-Fi 7. The L000659-02 antenna accommodates direct-to-access point mounting and upright or inverted orientations.
Applications for the L000659-02 include Wi-Fi 7 (802.11be), Wi-Fi 6E (802.11ax), Wi-Fi 6 (802.11ax), Wi-Fi 5 (802.11ac), Wi-Fi 4 (802.11n), 802.11b/g, WLAN, automation and control, outdoor and indoor applications.
To learn more, visit https://www.mouser.com/new/te-connectivity/te-l000659-02-wi-fi-6e-antenna/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.