Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

Mouser Now Stocking Texas Instruments' TPS25810 USB Type-C DFP Controller for Host Devices

January 6, 2016 - Mouser Electronics, Inc. is now stocking the TPS25810 USB Type-C™ downstream-facing port (DFP) controller from Texas Instruments (TI). The highly integrated TPS25810 controller provides all the functionality necessary to support a USB Type-C DFP (host) in a system that does not have USB Power Delivery (PD) source capabilities. The controller is ideal for systems such as a USB Type-C host port in notebook computers for sleep charging, LCD monitor/docking station and charging cradles, and USB Type-C wall chargers.

The TPS25810 USB Type-C DFP controller, now available from Mouser Electronics, monitors the two configuration channel (CC) pins to determine when a USB device is attached as well as the device orientation. The TPS25810 also identifies when Type-C audio or debug accessories are attached. The TPS25810 integrates a 3A, 34-mOhm power switch, which has two selectable fixed current limits (1.5A or 3A) that align with the Type-C current levels. The controller applies power to VBUS when it detects an upstream-facing port (UFP), and applies power to VCONN when it detects a powered cable. The controller also offers overcurrent or over-temperature protection, as well as power management to multiple high-current Type-C ports when all ports cannot simultaneously provide high current.

The TPS25810 draws less than 0.7µA (typical) when no device is attached. The controller offers additional system power savings in low-power states (S4/S5) by running from an auxiliary supply (AUX) which can lower the supply voltage from 5.5V to 3.3V.

The TPS25810 module is supported by the TPS25810EVM-745 Evaluation Module, which contains inputs and outputs as well as several test points and jumpers for easy configuration and evaluation of the TPS25810 features.

To learn more, visit http://www.mouser.com/new/Texas-Instruments/ti-tps25810-controller/.


With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Vice President, Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room