Now at Mouser: Qorvo QPQ1298 High-Performance BAW Filter for Sub Band 41 5G Network Infrastructure
May 19, 2021 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the QPQ1298 bulk acoustic wave (BAW) filter from Qorvo®. The QPQ1298 is a high-performance BAW 5G filter designed for sub-Band n41 uplink and downlink in base station infrastructure, small cell, and repeater applications.
The Qorvo QPQ1298, available from Mouser Electronics, features low insertion loss and high attenuation, vital for coexistence of 5G cellular bands and Wi-Fi operation in high-data-capacity rural, suburban, and dense urban areas. The QPQ1298 offers single-input and single-output operation in the 160 MHz bandwidth, with frequency ranges from 2515 MHz to 2675 MHz, to address n41 design challenges with bandwidth and Wi-Fi rejection, with no external matching required. Its three-pin 2.00 mm × 1.60 mm × 0.73 mm SMT package also provides engineers with a small-form-factor solution to simplify assembly.
Also available from Mouser is the QPQ1298EVB evaluation board, which features a pre-mounted QPQ1298 filter along with two 50Ω SMA connectors for RF in and RF out. The evaluation board provides an example application circuit, allowing rapid prototyping when incorporated into existing designs.
To learn more about the QPQ1298, visit https://www.mouser.com/new/qorvo/qorvo-qpq1298-baw-filter/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.