Toshiba’s Thermoflagger Over-Temperature ICs, Now Available at Mouser, Detect Temperature Increases in Electrical Equipment

New Product Announcement

Connect With Us


October 11, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the ThermoflaggerTM Over-Temperature ICs from Toshiba. Designed to detect and protect against abnormal heat generation, the Thermoflagger ICs allow engineers to configure over-temperature detection for an entire electronic product easily. The Thermoflagger Over-Temperature ICs help reduce size and power consumption for various applications, including mobile devices, home appliances, and industrial equipment.

The Toshiba Thermoflagger Over-Temperature ICs, now available at Mouser, are designed to be connected in series with positive temperature coefficient (PTC) thermistors placed near heat sources. The Thermoflagger ICs monitor resistance over the thermistors, which increases exponentially in the event of over-temperature. Connecting PTC thermistors in series enables over-temperature detection for multiple locations.

The compact, highly efficient Thermoflagger ICs offer low power consumption of 11.3 μA, while the standard SOT-553 package makes them a suitable choice for consumer electronic devices such as laptops and mobile devices. The Thermoflagger ICs feature an operating supply voltage range of 1.7 V to 5.5 V, a detect voltage range of 0.36 V to 0.64 V, and an operating temperature range of -40°C to +125°C. The over-temperature ICs offer a high PTCO output current accuracy of ±8%, as well as a selectable PTCO output current.

To learn more about the Toshiba Thermoflagger Over-Temperature IC, visit https://www.mouser.com/new/toshiba-semiconductors/toshiba-tcth0-ics/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Toshiba

2026 - Toshiba Electronic Devices & Storage Corporation (TDSC) offers a broad IC and discrete product line-up which includes Power, Small Signal, Optoelectronics, and Logic devices for automotive, multimedia, industrial, telecoms, and networking applications. TDSC develops, manufactures, and supplies innovative storage products including Enterprise and Consumer HDDs.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764