Texas Instruments LP5899-Q1 Automotive LED Driver, Now Available at Mouser, Supports SPI-Compatible Connectivity

New Product Announcement

Connect With Us


March 19, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the LP5899-Q1 automotive LED driver from Texas Instruments. The SPI-compatible device features an internal oscillator for generating the continuous clock required by the LP589x-Q1 family. The LP5899-Q1 LED driver is AEC-Q100 qualified for automotive applications and ideal for SPI-compatible connectivity in LP5891-Q1 and LP5892-Q1 devices.

The Texas Instruments LP5899-Q1 automotive LED driver, now available at Mouser, enables control of the LP589x-Q1 device family using a standard SPI controller. The LP589x-Q1 device family includes the LP5891-Q1, a highly integrated, common-cathode LED matrix driver for use in luminous LED panels, local dimming backlights, and other automotive applications. The LP5899-Q1 LED driver improves system reliability by incorporating fault reporting for the LP589x-Q1 daisy chain and LP5899-Q1 internal operations. Diagnostic features include open-drain FAULT pin, SPI communication loss detection, CRC for SPI communication, and CCSI data integrity.

The LP5899-Q1 device can drive multiple LED drivers from the LP589x-Q1 family, with the maximum number of cascaded devices determined by the LED driver. The LP5899-Q1 driver features an operating temperature range of -40°C to 125°C temperature range, making it a suitable choice for demanding automotive environments.

To learn more, visit https://www.mouser.com/new/texas-instruments/ti-lp5899-q1-led-drivers/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764