Mouser Now Shipping STMicroelectronics ST25R100 and ST25R200 NFC/HF RFID Readers for Read Plus Tag Applications

For Immediate Release

Connect With Us


September 10, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the ST25R100 and ST25R200 NFC/HF RFID readers from STMicroelectronics. STMicroelectronics ST25R100 AND ST25R200 near field communication, high frequency (NFC/HF), radio identification (RFID) reader integrated circuits (ICs) deliver high-end performance in a compact package for reader plus tag solutions in consumer, medical and industrial battery-powered applications.

The STMicroelectronics ST25R100 and ST25R200, available from Mouser, come in a small 4mm x 4mm 24-pin TQFN package offering high dynamic power output (0.8V/1.2W) for easy integration into applications with long-read range, small antennas and improved low-power card detection. The ST25R100 reader IC provides an entry-level option for cost-sensitive applications with a radio-controlled (RC) oscillator and a programmable timer to automatically scan for cards or other NFC-enabled devices while in wake-up (WU) mode. This IC is ideal for accessory recognition, automatic parameter setting, identification or access control with data transfer speeds of up to 6Mbit/s at 0.8V output power, external communication interfaces including a serial peripheral interface (SPI), and a wide 2.7V to 5.5V power supply range with an equally wide -25°C to 85°C ambient temperature range.

The ST25R200 reader IC adds extended features for medium to high-power applications like industrial IoT and gaming with integrated electromagnetic device (EMD) handling, active wave shaping (AWS) with overshoot or undershoot protection, and an RC oscillator with a programmable timer to scan for cards or other NFC-enabled devices while in WU mode. The ST25R200 also offers a serial peripheral interface (SPI) with data transfer speeds of up to 10Mbit/s with a 1.2W output power, a wide 2.7V to 5.5V power supply range with a broad -40°C to 85°C ambient temperature range.

To learn more about the ST25R100, visit https://www.mouser.com/new/stmicroelectronics/stm-st25r100-nfc-hf-rfid-reader-ic/.

To learn more about the ST25R200, visit https://www.mouser.com/new/stmicroelectronics/stm-st25r200-nfc-hf-rfid-reader-ic/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About STMicroelectronics

2026 - STMicroelectronics is a global independent semiconductor company and a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions, STMicroelectronics is at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence trends.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764