New at Mouser: STMicroelectronics’ ISM330IS and ISN330ISN iNEMO Inertial Modules for Industrial and IoT Applications
April 17, 2022 – Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is now stocking the ISM330IS and ISN330ISN iNEMO inertial modules from STMicroelectronics. The modules offer an integrated, system-in-package solution combining a three-axis digital accelerometer and three-axis digital gyroscope. The inertial modules enable always-on, low-power features for optimal performance in industrial and Internet of Things (IoT) applications, including industrial robots, asset tracking, condition monitoring, and complex motion detection.
The STMicroelectronics ISM330IS and ISN330ISN iNEMO inertial modules, now available at Mouser, feature an embedded intelligent sensor processing unit (ISPU), an ultra-low-power programmable core capable of executing signal processing and AI algorithms on the edge. The inertial modules offer a full-scale acceleration range of ±2 g to ±16 g and an angular rate range of ±125 dps to ±2000 dps. The modules’ ISPU utilizes data from the internal accelerometer/gyroscope and up to four external sensors using the device’s sensor hub functionality. The ISM330IS inertial module leverages an extensive ecosystem of libraries, as well as third-party tools and an integrated development environment (IDE). The ISM330ISN is paired with the NanoEdge.AI Studio, a developer tool from STMicroelectronics that allows users to create machine learning libraries.
The ISM330IS and ISN330ISN iNEMO Inertial Modules from STMicroelectronics are supported by the STEVAL-MKI233KA IS330IS evaluation kit. The evaluation kit includes a target board with a pre-mounted IS330IS sensor and an adapter card that enables connection to the STEVAL-MKI109V3 MEMS development platform (not included). The STEVAL-MKI109V3 MEMS development platform features a high-performance 32-bit microcontroller that functions as a bridge between the sensor and a PC, on which it is possible to use a downloadable graphical user interface (Unico-GUI) or dedicated software routines for customized applications.
To learn more about the ISM330IS and ISN330ISN iNEMO inertial modules from STMicroelectronics, visit https://www.mouser.com/new/stmicroelectronics/stm-ism330is-inemo-module/.
To learn more about the STEVAL-MKI233KA IS330IS evaluation kit, visit https://www.mouser.com/new/stmicroelectronics/stm-steval-mki233ka-kit/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.