Mouser Electronics Now Shipping Sensirion SFM3003 and SFM3013 Flow Meters for Medical Applications
December 6, 2021 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, offers the complete SFM series of digital flow meters from Sensirion, including the SFM3003 and SFM3013 flow meters.
SFM3003 and SFM3013 meters are versatile, bidirectional flow meters with low pressure drop, offering a large flow range of up to 300 standard liters per minute (SLM). These next-generation flow meters feature a digital I²C interface and Sensirion’s patented CMOSens® technology, which combines a thermal sensor element, signal processing, and digital calibration on a single microchip for fast signal processing.
The SFM3003 series provides additional features for measuring flows of air, oxygen, and air/oxygen mixtures. SFM3013 digital mass flow meters are based on the SFM3003 solution but feature robustness to overpressure (up to 1 bar gauge pressure) and are calibrated for air, oxygen, and air/oxygen mixtures. The SFM3013 series can also be calibrated for heliox gas mixtures.
Both meters are ideal for a variety of medical and industrial applications, including ventilation, anesthesia, inhalers, spectroscopy, and more. For development, Mouser also stocks the SEK-SFM3003 and SEK-SFM3013 evaluation kits, which work with the SEK-SensorBridge (sold separately) and include a flow sensor, connector cable, and downloadable SEK-ControlCenter software.
To learn more about the SFM3003 meter, visit https://www.mouser.com/new/sensirion/sensirion-sfm3003-flow-meters/.
For more information on the SFM3013 meter, go to https://www.mouser.com/new/sensirion/sensirion-sfm3013-flow-meters/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
2026 - Sensirion is a leading sensor manufacturer, providing relative humidity sensors and flow sensor solutions with unique performance. The company's product range includes liquid flow sensors, mass flow meters, mass flow controllers and differential pressure sensors. Using Sensirion's microsensor solutions, OEM customers benefit from the proven CMOSens® technology and excellent technical support. Among a large variety of applications, flow and humidity sensors are successfully used in the automotive and medical industries.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.