Schneider Electric Altivar ATV350 Variable Speed Drives, Now at Mouser, Offer On-Machine Mounting in Warehouse and Distribution Environments

New Product Announcement

Connect With Us


Learn more about the  Altivar ATV350 VSDs
Learn more about the Altivar ATV350 VSDs

October 7, 2026 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the Altivar ATV350 variable speed drives from Schneider Electric. The Altivar ATV350 variable speed drives (VSDs) are designed for on-machine mounting with IP66/NEMA4X or IP54/NEMA12 protection for 460 V motors up to 15 hp. The new on-machine ATV350 VSDs are suitable for material handling in logistics, food and beverage, consumer packaged goods (CPG), and airport environments.

The Schneider Electric Altivar ATV350 variable-speed drives, now available at Mouser, mount directly onto conveyor systems, lowering overall costs and reducing wiring complexity and installation time. With daisy-chain network connectivity for Ethernet/IP, PROFINET, EtherCAT, and Modbus TCP, the Altivar ATV350s integrate seamlessly into existing control architectures. The Altivar ATV350's plug-and-play and poka-yoke hardware design minimizes the risk of wiring errors, while user-friendly software allows for remote configuration, control, and monitoring. The Altivar ATV350 VSDs can control synchronous and asynchronous motors with heavy-duty performance, and the enclosure-free design with IP66 and UL Type 4X rating ensures reliable operation in environments exposed to dust, moisture, or washdown procedures. Featuring a small form factor, the Altivar ATV350 VSDs are also suitable for space-constrained environments.

 

The Altivar ATV350 VSDs include Safe Torque Off (STO) up to a SIL3 rating, with either hardwired or network-based safety integration. The Altivar ATV350 variable speed drives feature a 0.75kW to 11kW (1hp to 15hp) power range, a 380V to 480V voltage range, and an operating temperature range of  -30°C to +40°C without derating or +40°C to +60°C with derating.

To learn more, visit https://www.mouser.com/new/schneider-electric/schneider-altivar-atv350-speed-drives/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

Mouser offers thousands of industrial automation products, in stock and available for immediate shipping. From predictive maintenance and control panel devices to a full range of industrial power, sensor, and safety products, Mouser's portfolio is available to help customers design, build and maintain complete automation solutions. To learn more, visit https://www.mouser.com/solutions/industrial-automation/ and follow Mouser on Facebook, LinkedIn, X, and YouTube.

 

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Schneider Electric

2026 - Schneider Electric, a global specialist in energy management with operations in more than 100 countries, offers integrated solutions across multiple market segments, including leadership positions in energy and infrastructure, industrial processes, building automation, and data centers/networks, as well as a broad presence in residential applications.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764