Mouser Electronics Signs Global Distribution Deal with Sanan Semiconductor, Expanding SiC Industrial and Automotive Power Portfolios

For Immediate Release

Connect With Us


July 11, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announces a global distribution agreement with Sanan Semiconductor, a leading manufacturer of silicon carbide (SiC) power products, including industrial and automotive SiC Schottky barrier diodes (SBDs) and SiC MOSFETs. Sanan Semiconductor offers flexible solutions for high-power and high-reliability applications, such as server power supplies, photovoltaic inverters, electric vehicles, and home appliances.

Sanan Semiconductor’s industrial SiC Schottky barrier diodes offer higher efficiency, greater heat dissipation capability, and lower losses than traditional silicon-based solutions. These features enable higher power density and longer-term reliability in system designs. These devices show no recovery at turn-off and allow a low leakage current with a reverse voltage of up to 1200V. Utilizing an innovative merged PiN Schottky (MPS) structure and substrate thinning technology, these SiC SBDs offer compelling price performance while meeting the industry’s most stringent reliability requirements. Sanan Semiconductor’s SiC SBDs also maintain consistent performance over a broad temperature range, simplifying system design.

Sanan Semiconductor’s automotive SiC Schottky barrier diodes are RoHS-compliant and AEC-Q101 qualified, making them ideal for use in automotive applications. These automotive SiC components offer superior power handling due to their high voltage and current ratings, enabling high frequency and high-temperature operation, which boosts power density, efficiency, and system compactness. These devices offer a greatly reduced capacitive charge (Qc), which minimizes reverse recovery loss and aids in fast switching.

Both grades of SiC SBDs are offered in a diverse range of packaging options to suit every need. From standard Transistor Outline (TO) packages to Surface Mount Device (SMD) solutions and bare die, Sanan Semiconductor’s packaging options are engineered for versatility and performance.

To learn more, visit https://www.mouser.com/manufacturer/sanan-semiconductor/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Sanan Semiconductor

2026 - Sanan Semiconductor started production in Xiamen, China, in 2014. The company has a robust megafab Silicon Carbide (SiC) capacity, ranking among the top three worldwide. Sanan Semiconductor is committed to cutting-edge technology and uncompromising quality, which positions it as a leader in the global semiconductor market. At the heart of the company's operations is a comprehensive suite of foundry solutions meticulously designed to ensure the security and resilience of the Silicon Carbide (SiC) and Gallium Nitride (GaN) supply chain.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764