New at Mouser: ROHM TLR377GYZ CMOS Op Amp Optimized for Smartphones and Ultra-Compact IoT Devices

New Product Announcement

Connect With Us


September 16, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the miniaturized TLR377GYZ CMOS operational amplifier (op amp) from ROHM Semiconductor. The ultra-small 0.88 mm x 0.58 mm device is optimized for amplifying signals from sensors such as temperature, pressure and flow rate, used in smartphones, small Internet of Things (IoT) devices and similar applications.

The TLR377GYZ op amp, available from Mouser, balances miniaturization with high accuracy by leveraging ROHM's proprietary circuit design, process and packaging technologies. The device offers a maximum offset voltage as low as 1 mV and an input equivalent noise voltage density as low as 12nV/√Hz. Furthermore, the TLR377GYZ op amp adopts a WLCSP (wafer-level chip scale package) with a ball pitch of just 0.3 mm utilizing original packaging technology. This package design reduces size by approximately 69% compared to conventional products and 46% over existing compact products.

The TLR377GYZ also features a built-in shutdown function, which limits the device's operation to sensing-only periods. This feature significantly reduces standby current to a maximum of 1.5 µA.

The TLR377GYZ op amp is supported by the TLR377GYZ-EVK-001 evaluation board. The TLR377GYZ-EVK-001 provides a pre-mounted TLR377GYZ Op Amp mounted on a 2.4 mm x 2.4 mm x 1.0 mm PCB. This conversion board can replace SSOP6 packages, enabling evaluation in existing designs.

To learn more about the TLR377GYZ op amp, visit https://www.mouser.com/new/rohm-semiconductor/rohm-tlr377gyz-amplifier/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About ROHM Semiconductor

2026 - ROHM Semiconductor designs and manufactures semiconductors, integrated circuits, and other electronic components for the wireless, computer, automotive, and consumer electronics markets. ROHM Semiconductor's comprehensive product portfolio covers everything from audio/video ICs, wireless audio links, image sensors, and noise protection discretes to memory products  featuring double-cell technology, energy-efficient power management components, LEDs, and more.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764