Mouser Now Shipping Renesas RL78/G23 Low-Power MCUs with New Capacitive Touch Unit

New Product Announcement

Connect With Us


June 10, 2021Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the RL78/G23 microcontroller from Renesas Electronics. The RL78/G23 microcontroller is compatible with Renesas’ RL78 family of microcontrollers, offering engineers increased 16-bit performance and lower power consumption for a host of consumer and industrial Internet of Things (IIoT) applications.

Utilizing new processes and functionality, the Renesas RL78/G23 microcontroller, available from Mouser Electronics, expands peripheral features and efficiency while lowering power consumption, making it suitable for a wide range of applications, from home appliances and consumer electronics to industrial automation. The device consumes just 44 µA/MHz at CPU operation and 210 nA in STOP mode (with 4 Kbytes of SRAM retention), offering improved performance compared to current series microcontrollers. A newly implemented snooze mode sequencer (SMS) makes it unnecessary to activate the CPU while peripheral operations are in snooze mode, dramatically improving efficiency for applications that require intermittent operation.

The RL78/G23 features a wide operating voltage range of 1.6 V to 5.5 V up to 32 MHz, with 768 Kbytes of on-chip flash memory capacity. The device’s logic and event link controller (ELCL) makes it possible to create conditional links to multiple events while continuing to benefit from the reduced power consumption realized by the conventional event link controller (ELC). The RL78 family’s first capacitive touch-sensing unit (CTSU2L) combines exceptional high-sensitivity and low-noise characteristics, which can be used to implement a contactless gesture-based user interface, ideal for consumer and industrial control surfaces.

The RL78/G23 Fast Prototyping Board, also available at Mouser Electronics, is designed for prototyping various applications using the RL78/G23 microcontroller. The board comes standard with Arduino Uno and Grove interfaces for simplified programming and offers high scalability with access to all pins on the microcontroller.

To learn more about the RL78/G23 microcontroller, visit https://www.mouser.com/new/renesas/renesas-rl78-g23-mcus/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764