Now at Mouser: Renesas’ High-Performance FemtoClock2 Synthesizers for Programmable Fiber Optic Modules

New Product Announcement

Connect With Us


September 30, 2021Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the FemtoClock2 high-performance clock-frequency synthesizers from Renesas Electronics. Featuring jitter as low as 64fs RMS maximum, the FemtoClock2 synthesizers are designed to be placed adjacent to a switch, ASIC, FPGA, or PHY that requires several reference clocks with less than 100fs maximum jitter performance. Additionally, the high-performance devices can be used as an adjustable OTN clock reference for OTU3/OTU4 mappers, as well as a reference clock for programmable fiber optic modules.

The Renesas FemtoClock2 synthesizers, available from Mouser Electronics, consist of the RC22504A synthesizer and RC32504A jitter attenuator and synthesizer. The devices can also act as a DCO for frequency margining or OTN clock applications. The devices’ PLL core consists of fractional-feedback analog PLL (optionally steered by a digital PLL in the RC32504A device) and operates from a crystal with frequencies between 25 MHz to 80 MHz.

The FemtoClock2 synthesizers feature four differential or eight LVCMOS outputs, supporting any frequency from 10 MHz to 1 GHz (180 MHz for LVCMOS). The versatile synthesizers can configure themselves automatically after reset, using an internal customer-definable one-time programmable memory with up to four different configurations.

The FemtoClock2 synthesizers are supported by the RC22504A evaluation kit. Engineers can develop configurations using Renesas RICBox software and then upload to the evaluation board using a USB connection. The evaluation kit features Renesas low-noise power supply regulators and a Renesas low-noise fan-out buffer.

To learn more about the Renesas FemtoClock2 synthesizers, visit https://www.mouser.com/new/renesas/renesas-rc22504a-synthesizer/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764