Mouser Now Shipping UnitedSiC (Now Qorvo) 750V UJ4C/SC SiC FETs in D2PAK-7L Package for Industrial Applications

New Product Announcement

Connect With Us


September 8, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the UJ4C/SC FETs from UnitedSiC (now Qorvo®) in an industry-standard, D2PAK-7L surface-mount package. The UJ4C/SC series devices are 750 V silicon carbide field-effect transistors (SiC FETs) that capitalize on the D2PAK-7L package option to deliver low switching loss, increased efficiency at higher speeds, and improved system power density. The FETs are optimized for applications such as onboard chargers, soft-switched DC/DC converters, battery charging, and IT/server power supplies.

The UJ4C/SC devices, available from Mouser Electronics, leverage a unique cascode SiC FET technology in which a normally on SiC JFET is co-packaged with a silicon MOSFET to produce a normally off SiC FET. The FETs reduce inductance from compact internal connection loops, which, along with the included Kelvin source connection, results in low switching loss, enabling higher frequency operation and improved system power density.

The D2PAK-7L version of the UJ4C/SC series is available in on-resistance options from 9 mΩ to 60 mΩ, delivering design flexibility while maintaining generous design margins and circuit robustness. Rated to 750 V, the FETs offer a best-in-class on-resistance × area (RDS(on) × A) figure of merit and a low body diode, ultra-low gate charge, and a 4.8 V threshold voltage that allows a gate drive of 0 V to 15 V for ultimate versatility with low conduction losses.

To learn more, visit https://www.mouser.com/new/unitedsic/unitedsic-uj4c4s-750v-gen4-sic-fets/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764