Mouser Electronics Now Stocks Qorvo QPF7551 & QPF7552 Wi-Fi 6 FEMs with bandBoost Technology for Mesh Home Networks

New Product Announcement

Connect With Us


January 6, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the QPF7551 and QPF7552 integrated front-end modules (iFEMs) from Qorvo®. Providing reliable, whole-home coverage when designed into Wi-Fi 6 (802.11ax) systems, the iFEMs incorporate Qorvo’s advanced bulk acoustic wave (BAW) filter technology with unique bandBoost™ capability, which enables consumers to fully enjoy the speed advantages of mesh home networks that broadcast concurrently on three different channels.

The Qorvo QPF7551 and QPF7552 Wi-Fi 6 iFEMs, available from Mouser Electronics, integrate a 5 GHz power amplifier (PA) optimized for a 5 V supply voltage, which saves power while maintaining high linear output power. Qorvo’s bandBoost filtering technology maximizes capacity and range by boosting band isolation in distributed Wi-Fi 6 systems.

In addition to the PA and filter, the modules include a bypassable low-noise amplifier (LNA) and a single-pole, two-throw (SP2T) switch in a single module, which reduces board size by as much as 30% and simplifies design requirements. The modules also offer 5 GHz rejection for dual-band dual-concurrent (DBDC) operation, as well as integrated die-level filtering for second and third harmonics.

The QPF7551 and QPF7552 iFEMs are ideal for a range of connectivity solutions, including wireless routers, access points, residential gateways, Wi-Fi customer premises equipment, and Internet of Things (IoT) applications. For development, the QPF7551EVB and QPF7552EVB evaluation boards are available to order from Mouser.

To learn more about the QPF7551 iFEM, visit https://www.mouser.com/new/qorvo/qorvo-qpf7551-fem/.

For more information about the QPF7552 iFEM, go to https://www.mouser.com/new/qorvo/qorvo-qpf7552-ifem/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764