Mouser Now Shipping Qorvo QPF4532 Integrated Front End Module for Wi-Fi 6 Designs
June 7, 2022 – Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is now shipping the QPF4532 Wi-Fi 6 integrated front end module (FEM) from Qorvo®, designed for the latest Wi-Fi 6 (802.11ax) systems such as residential gateways, wireless routers, access points and Internet of Things (IoT) applications.
The Qorvo QPF4532 FEM, available from Mouser Electronics, integrates a 5.0 GHz power amplifier (PA), single-pole, two-throw (SP2T) switch and bypassable low noise amplifier (LNA) into a single device. With a compact form factor and integrated matching that minimizes layout area in the application, performance of the QPF4532 is focused on optimizing the PA for a 3.3 V supply voltage to conserve power consumption, while maintaining the highest linear output power and leading-edge throughput. Receive path design matches optimal technologies to maximize receive sensitivity through noise figure performance as low as 2 dB, for consistency over a wider variety of conditions.
The QPF4532 features integrated die-level filtering for second and third harmonics as well as 2.4 GHz rejection for dual-band, dual-concurrent (DBDC) operation. For application feedback, a DC power detector is integrated into the halogen- and lead-free package to provide voltage that is proportional to the output power from the transmit path.
For development, Mouser also stocks the QPF4532EVB evaluation board, which provides an example application circuit to allow rapid prototyping when incorporated into existing designs.
To learn more about the QPF4532, visit https://www.mouser.com/new/qorvo/qorvo-qpf4532-wifi-6-front-end-module/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.