Mouser Now Stocking Qorvo QPA1314T 55 W GaN Power Amp for RF Satellite Communication

New Product Announcement

Connect With Us


September 15, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the QPA1314T power amplifier (PA) from Qorvo®. Manufactured using Qorvo’s production 0.15 μm gallium nitride-on-silicon carbide (GaN-on-SiC) process (QGaN15) and mounted to a high thermal conductivity tab, the QPA1314T is a high-power MMIC amplifier ideal for commercial and defense RF communication applications.

The Qorvo QPA1314T PA, available from Mouser Electronics, features an extended frequency range of 12.75 to 15.35 GHz and achieves 55 W of saturated output power in its standard range of 13.75 to 14.5 GHz. The device integrates DC blocking capacitors on both the input and output ports and is fully matched to 50 ohms to simplify system integration. The PA’s RF ports are also DC coupled to ground to achieve optimal ESD performance.

Optimized for RF satellite and radar communications and datalinks in commercial and military markets, the QPA1314T is lead-free, halogen-free, RoHS compliant, and 100% DC and RF tested on-wafer to ensure compliance to electrical specifications. For evaluation and development, Mouser also offers the QPA1314DEVB evaluation board.

To learn more, visit https://www.mouser.com/new/qorvo/qorvo-qpa1314t-amplifer/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764