Mouser Now Shipping New NXP Semiconductors Ara240 Discrete Neural Processing Unit for AI, Edge, Industrial, and Robotics Applications
October 5, 2026 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the new Ara240 discrete neural processing unit (DNPU) from NXP® Semiconductors. The Ara240 DNPU enables real-time generative AI, industrial automation systems, autonomous robots, smart infrastructure, advanced machine interface (HMI) platforms or edge applications.
The Ara240 DNPU, available from Mouser, combines balanced compute and high off-chip bandwidth to efficiently execute large language models (LLMs) and vision-language models (VLMs), while delivering low latency, lower operational costs, and enhanced data privacy. The Ara240's innovative architecture is designed to support advanced multimodal and transformer-based workloads, achieving up to 40 equivalent tera-operations per second (eTOPS) and supporting up to 16 GB of LPDDR4 memory. This feature enables smooth execution of large and complex models directly at the edge, without reliance on high-cost cloud compute resources.
With integrated secure boot and a hardware root-of-trust processor, the Ara240 DNPU provides hardened security for industrial, enterprise, and embedded deployment environments. Its PCIe Gen4 and USB 3.2 host interfaces allow straightforward integration into edge compute platforms, PCs/laptops, and AI-enabled embedded systems. Whether designing industrial automation systems, autonomous robots, smart infrastructure, advanced human‑machine interface (HMI) platforms or edge servers, the Ara240 DNPU provides the performance headroom needed to run modern AI workloads directly at the edge.
Complementing the Ara240 DNPU is the full-featured Ara SDK, which accelerates AI application development and simplifies deployment of diverse AI workloads across Ara240-based DNPUs and modules.
The Ara SDK features an extensible AI compiler to support diverse and evolving model architectures, including convolutional and fully connected neural networks (CNNs), vision transformers (ViTs), as well as highly complex language models like LLMs and VLMs. The SDK offers efficient dataflow optimization, flexible quantization methods and support for multiple datatypes, ensuring high-performance and low-latency for edge-AI applications.
The ARA2-M2-16G-GT, also available from Mouser, is an AI accelerator module based on the Ara240 DNPU. It uses the M.2 M-Key design specifications and supports up to four PCI Express 4.0 lanes in x4 configuration. Designed with the commonly used NGFF 2280 form factor, it can be easily used as a companion processing unit with the FRDM i.MX 95 and FRDM i.MX95 Pro development boards with M.2 M-Key PCI Express capability.
To learn more, visit https://www.mouser.com/new/nxp-semiconductors/nxp-ara240-discrete-neural-processing-units/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.
Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.