Nordic Semiconductor's Thingy:53 Platform, Now Available at Mouser, Enables Rapid Prototyping of Wireless Devices with ML Capabilities

For Immediate Release

Connect With Us


Month 07, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the Thingy:53 rapid prototyping platform from Nordic Semiconductor. Integrating a range of sensors for light, motion, sound, and environmental factors, the Thingy:53 platform provides an ideal solution for building prototypes and proofs-of-concept.

The Thingy:53 Rapid Prototyping Platform is based on the nRF5340 dual-core Arm® Cortex® M-33 system-on-chip (SoC), and the nRF Edge Impulse mobile app enables embedded machine learning (ML) for prototype devices. The platform's ML capabilities support a range of applications, including voice recognition and movement pattern detection.

The Nordic Semiconductor Thingy:53 rapid prototyping platform features a complete range of sensors and peripherals to support Internet of Things (IoT) application development. The platform's environmental sensor measures air pressure, air quality, humidity, and temperature in real time, while the low-power accelerometer supports a broad range of motion detection functions. The platform also offers a connector for external accessories and boards, further extending the possible applications for prototype devices.

The Thingy:53 platform boasts power management features provided by the nPM1100 power management IC (PMIC), an onboard nRF21540 front-end module (FEM) for wireless connectivity and an integrated power amplifier/low noise amplifier (PA/LNA) range extender. The platform's ML capabilities enable exceptional low-power performance, as devices can conserve battery life when no external stimuli trigger the embedded sensors. The Thingy:53 rapid prototyping platform includes a debug and current measurement board, allowing engineers to monitor power consumption and troubleshoot application code quickly.

To learn more about the Thingy:53 rapid prototyping platform from Nordic Semiconductor, visit https://www.mouser.com/new/nordic-semiconductor/nordic-thingy-53-platform/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Nordic Semiconductor
2026 - Nordic Semiconductor is a fabless semiconductor company specializing in wireless communication technology that powers the IoT. The company's award-winning Bluetooth Low Energy solutions pioneered ultra-low power wireless, making Nordic the global market leader. The company's development tools shield the developers from RF complexity, allowing anyone with a bright idea to build innovations based on the IoT platform. Today, Nordic's award-winning, high-performance, yet easy to design-in, Bluetooth LE, cellular IoT, and Wi-Fi solutions are used by the world's leading brands in a variety of products, including advanced wearables, smart home, medical, industrial automation, sports and fitness, logistics and transportation, etc..
Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764