Mouser Now Offering Crocus CT430, CT431 & CT450 XtremeSense TMR Sensors

New Product Press Brief

Connect With Us


February 16, 2022 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now offering CT430, CT431, and CT450 XtremeSense® tunnel magnetoresistance (TMR) sensors from Crocus Technology.

Crocus Technology CT430 and CT431 XtremeSense TMR sensors are high-bandwidth and ultra-low-noise integrated contact current sensors. The sensors use Crocus’ patented XtremeSense TMR technology to enable high-accuracy current measurements for many consumer, enterprise, and industrial applications.

The CT430 and CT431 sensors support six current ranges. The integrated current-carrying conductor (CCC) handles up to 50 A of current and generates a current measurement as a linear analog output voltage. The device delivers a total output error of less than ±1.0% full-scale (FS) over voltage and the full temperature range. Additionally, the sensors achieve less than 1.0 µs output response time, with current consumption of about 6.0 mA that immune to common mode fields.

The Crocus CT450 is a high-bandwidth, low-noise integrated contactless current sensor with XtremeSense TMR technology to enable high-accuracy current measurements. The sensor supports eight field ranges, sensing and translating the magnetic field into a linear analog output voltage. The CT450 device features a total error output of less than ±1.0% over voltage and temperature, with an output response time of less than 1.0 µs and current consumption of approximately 5.0 mA.

Applications for all three series of sensors include solar and power inverters, smart appliances, motors and generators, power supplies, battery management, and power utilities.

To learn more about the CT430, visit https://www.mouser.com/new/crocus-technology/crocus-ct430-sensors/.

To learn more about the CT431, visit https://www.mouser.com/new/crocus-technology/crocus-ct431-sensors/.

For more information about and CT450, go to https://www.mouser.com/new/crocus-technology/crocus-ct450-sensors/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764