Banner Engineering’s R130C IO-Link Hub, Now at Mouser, Enables Industrial Automation, Sensor, and IoT Applications

New Product Announcement

Connect With Us


May 20, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the R130C discrete IO-Link hub from Banner Engineering. The R130C IO-Link hub is a compact, top-exit IO-Link hub that allows connections for up to 16 non-IO-Link devices into an IO-Link system for industrial automation, sensor networks, supervisory control, data acquisition, and Internet of Things (IoT) applications.

Banner Engineering’s R130C 8-port discrete IO-Link hub, available from Mouser, utilizes industry-standard top-exit M12-connectivity and 16-discrete PNP inputs for efficient and cost-effective mounting on machines near sensors, resulting in fewer wires and space savings in control cabinets by eliminating costly PLC input cards. The R130C hub also provides power to other devices, with four amps shared across all eight ports, for lighting products and other devices without the use of splitters. The R130C also has I/O status LEDs, which are visible from the top or side of the device, greatly easing troubleshooting for the device, regardless of mounting location.

Mouser also stocks Banner Engineering’s R95C IO-Link hubs to convert and consolidate discrete and analog signals into an IO-Link or Modbus data stream. The R95C-8B21-KQ is a bimodal-to-IO-Link device converter that connects discrete inputs and sends the value to the IO-Link master. These hubs feature eight ports, four-pin M12 integral quick disconnects, and an IO-Link interface with two configurable I/O pins per port that support PNP or NPN inputs and outputs.

When combined with Banner’s IO-Link Masters, the R130C and R95C IO-Link hubs can transmit eight to sixteen signals via IO-Link to the customer’s human-machine interface (HMI), programmable logic controller (PLC), or other network devices. Each hub is equipped with eight industry-standard M12 ports, where the input ports can be customized individually.

To learn more about the R130C, visit https://www.mouser.com/new/banner-engineering/banner-r130c-io-link-hub/.

To learn more about the R95C, visit https://www.mouser.com/new/banner-engineering/banner-r95c-io-link-hubs/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Banner Engineering

2026 - Banner Engineering designs and manufactures industrial automation products, including sensors, smart IIoT and industrial wireless technologies, LED lights and indicators, measurement devices, machine safety equipment, barcode scanners, and machine vision. These solutions help make many of the things people use every day, from food and medicine to cars and electronics. A high-quality, reliable Banner product is installed somewhere around the world every two seconds. Headquartered in Minneapolis since 1966, Banner is an industry leader with more than 10,000 products, operations on five continents, and a worldwide team of more than 5,500 employees and partners. The company's dedication to innovation and personable service makes Banner a trusted source of smart automation technologies to customers around the globe.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764