Mouser Explores the World of 5G with Extensive Technical Resource Center and New Products for Engineers
May 16, 2024 – Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, provides engineers with insightful and trusted resources in its 5G content hub. Mouser’s technical resource center offers a wealth of knowledge about the expansion of the reliable low-latency network. This global wireless standard offers increased bandwidth, enabling devices to connect from further distances at faster speeds, as well as enhancing machine-to-machine contact for a connected future. These upgrades impact our everyday lives, like elevating public transportation through vehicle-to-vehicle communication and leveling up your smart home with improved IoT devices and faster service. The comprehensive resource center provides a library of curated products, tools, and content to support every aspect of the connectivity revolution.
The proliferation of IoT and the deployment of 5G are driving the evolution of edge computing and data center infrastructure to support ultra-reliable low-latency communication, massive machine-type communication, and enhanced mobile broadband services. The rollout is in tandem with the development of Industry 4.0, increasing the number of vulnerable online endpoints and the risk of cyberattacks. Engineers must be diligent about creating safer systems through risk management plans and promoting a cyber-secure culture.
The latest trends and updates to the technological standard are assembled in a one-stop hub for engineers to gain knowledge about every aspect of 5G. As it continues to transform various parts of our lives, Mouser partners with leading manufacturers to curate articles, blogs, eBooks, and products to build a fast and reliable connected world. In one of Mouser’s installments of the Empowering Innovation Together™ series, experts delve into the benefits private 5G networks bring to Industrial IoT, such as lower latency and machine-to-machine communication.
Mouser stocks the industry’s widest selection of electronic components and network products, including the following solutions for 5G applications:
- The QPB9380 dual-channel switch-LNA module from Qorvo is an RF front-end module (FEM) that integrates a two-stage LNA and a 20W power-handling switch in a dual-channel configuration. The device operates across the 2.3 GHz to 5 GHz frequency range and provides a 1 dB noise figure in a 6mm2 compact package. Typical applications include 5G radio, small cell BTS, and wireless infrastructure.
- FP90 4x4 MiMo antennas from TE Connectivity / Laird External Antennas are future-proofed against 4G and 5G frequency rollouts up to 7125 MHz. These antennas offer multiple connector options to suit all major vehicular gateways and routers. With IP67 ingress protection, they have an operating temperature range of -40°C to 85°C and customizable connector, cable length, and port configurations. The antennas are designed for various automotive applications, from public transport to emergency services.
- The SNYPER-5G Graphyte (GL) spectrum analyzer by Siretta is a high-performance, multi-language network signal analyzer and cellular signal logger. This spectrum analyzer is designed to survey the 5G NR, 4G LTE, LTE-M, NB-IoT, and 2G/GSM networks. Typical applications include evaluating the “preferred” network operators’ performance, determining optimum antenna placement, and enhancing cellular surveying of new and existing installations.
- The RUTX50 industrial 5G router from Teltonika is a multi-network industrial device enabling 5G mobile communication for high-speed and data-heavy applications. The router integrates 5G technology with various interfaces and industrial hardware features, resulting in future upgrade/expansion adaptability. It has a 5G dual SIM cellular communication merged with 5 Gigabit Ethernet ports and dual-band Wi-Fi®, enabling ultra-low latency data transfer. Compatible with the Remote Management System (RMS), the router is optimized for remote management and monitoring capabilities of large fleets of devices.
- 5G25 RF flex-to-board connectors by Molex feature a shield design that supports high-frequency signals up to 25 GHz. These connectors enable designers of RF antenna modules and mobile devices to combine RF and non-RF signals, reducing the need for additional connectors. The 5G25 connectors are suitable for consumer, industrial, medical, and defense applications.
To learn more, visit https://resources.mouser.com/5g/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.