Mouser Now Stocking ams OSRAM SYNIOS P3030 KW DSLP31.CE LED for Car Body Illumination

New Product Announcement

Connect With Us


October 4, 2022Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the SYNIOS® P3030 KW DSLP31.CE LED from ams OSRAM. Part of ams OSRAM's SYNIOS P Family of products, the P3030 KW DSLP31.CE delivers an exceptional solution that meets the energy efficiency, weight, and space-saving qualities for the rapidly emerging field of automotive exterior lighting.

The ams OSRAM SYNIOS P3030 KW DSLP31.CE, available from Mouser Electronics, is a white LED with a luminous flux/radiant flux of 45 lm to 71 lm and a minimum color rendering index (CRI) of 90. Forward current is rated at 3 mA to 200 mA, with a pulsed forward current of 400 mA (max.). The LED functions on a forward voltage of 2.6 V to 3.5 V, with a maximum reverse voltage of 5 V.

Incorporating InGaN-on-sapphire chip technology, the KW DSLP31.CE is designed using a colored-diffused silicone resin with a very flat square package. The close-to-center chip layout allows for optimal design flexibility, and its small outline dimensions, especially the height, provide maximum flexibility to accommodate even the tightest of spaces.

The compact 3 mm × 3 mm × 0.65 mm SMT LED operates at -40°C to +125°C and is ESD tested at 2 kV according to ANSI/ESDA/JEDEC JS-001 (HBM, Class 2). The LED is AEC-Q102 qualified and enables designers to incorporate design, comfort or safety functions using car-body illumination for a variety of automotive-based lighting applications.

To learn more, visit https://www.mouser.com/new/ams-osram/ams-osram-synios-p3030-kwdslp31ce-led/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About ams OSRAM

2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.

ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764