New at Mouser: ams OSRAM SPL S1L90H 1-Channel SMT Laser for Industrial LIDAR and Ranging Applications

New Product Announcement

Connect With Us


August 10, 2023Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the SPL S1L90H 1-channel SMT laser from ams OSRAM. The SPL S1L90H SMT laser gives engineers improved performance and easier optical integration for long-distance industrial ranging and LIDAR applications, such as drones and robots, as well as building and industrial automation. 

ams OSRAM's SPL S1L90H 1-channel SMT laser, available from Mouser Electronics, is a versatile, small aperture, edge-emitting laser (EEL) in a surface-mount (SMT) package with advanced chip technology. The SPL S1L90H features the highest peak power (65 W) and average power in the small package class. The device is one of the first surface-mount, edge-emitting lasers to have a 110 µm aperture, enabling a very narrow beam that is optimized for short-pulsed LiDAR applications.

The single-channel SPL S1L90H SMT Laser features ams OSRAM's multi-junction technology, consisting of three vertically stacked emitters in a single laser die mounted inside the device's 2.3 mm x 2.0 mm x 0.69 mm quad flat no-lead (QFN) package. This technology results in better target area illumination at long-range distance measurement, 3D optical sensing, and simultaneous localization and mapping (SLAM) applications.

The SPL S1L90H's optimized, power-efficient pulsed laser enables a maximum pulse width of 50 ns and is suitable for pulses shorter than 2 ns. Beam divergence is just 10° (parallel) x 25° (perpendicular), enabling efficient beam shaping with its small aperture. It is specified for corrosion robustness to class 3B, with low thermal resistance for a more straightforward system thermal design.

To learn more, visit https://www.mouser.com/new/ams-osram/ams-osram-spl-s1l90h-3-smt-laser/.

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About ams OSRAM

2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.

ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764