New at Mouser: Amphenol Industrial TS1 Series High-Power Connectors for Industrial, Transportation and Energy Applications

New Product Announcement

Connect With Us


Learn more about the TS1 series high-power connectors
Learn more about the TS1 series high-power connectors

August 24, 2026 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new TS1 series high-power connectors from Amphenol Industrial. The TS1 connectors are single-pole, metal-shell connectors with a robust latch designed for high-power electrified systems in industrial, transportation, commercial, and energy systems applications.

The Amphenol Industrial TS1 series, available from Mouser, is a sealed, high-voltage, high-current power connector platform designed to help designers deliver reliable electrification in harsh environmental conditions. Built for demanding duty cycles, the TS1 series is intended for high-power electrified and hybrid applications experiencing elevated thermal, mechanical, and electrical stresses. TS1 is built to support those realities with a rugged mechanical design and shielding features intended to help protect critical power links.

This high-voltage, high-current power connector platform helps engineers route power between batteries, inverters, PDUs, DC-DC converters, pumps, and drives, especially in environments where shock, vibration, and exposure can challenge connection integrity. These connectors include 8mm contacts rated up to 200A and 12mm contacts rated up to 450A, giving designers flexibility across a wide range of high-current architectures. The TS1 12 mm connectors are rated up to 2000 VDC, and the 8 mm versions are rated up to 1500 VDC, for high-voltage architectures. They accommodate 35 mm² to 120 mm² cables, including versions with individually shielded conductors.

The TS1 series is also well-suited for applications that require reliable power delivery while managing electromagnetic interference (EMI) generated by high-frequency switching devices. With a metal-shell design and sealing system, TS1 connectors achieve IP6K9K ingress protection, suitable for road spray and high-pressure washdown. They are rated for up to 500 mating cycles and validated to withstand 20G vibration and can operate over the -40°C to +125°C temperature range, making them appropriate for both under-hood and chassis-mounted applications.

To learn more, visit https://www.mouser.com/new/amphenol/amphenol-industrial-ts1-high-power-connectors/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Amphenol Industrial

2026 - Amphenol Industrial offers a wide variety of receptacles, plugs, and connectors. Amphenol Industrial has long been the accepted leader in providing quality connectors and interconnect systems to the industrial markets and is the leading manufacturer of cylindrical connectors in the world.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764