Murata SCH16T-K01 6-DOF Gyroscope, Now at Mouser Electronics, Enables High-Precision Machine Control and Positioning Applications

New Product Press Brief

Connect With Us


July 25, 2024 - Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the SCH16T-K01 6-DoF gyroscope by Murata Electronics.

Murata Electronics SCH16T-K01 gyroscope is AEC-Q100 qualified and combines three-axis angular rate and three-axis accelerometers with a digital SPI interface. The angular rate and accelerometer sensor elements are built on Murata's capacitive 3D-MEMS technology, and the signal processing is completed by a single mixed-signal ASIC that provides angular rate and acceleration via a flexible SafeSPI v2.0 compliant digital interface. This device features a ±300°/s calibrated angular rate measurement range, ±80m/s2 calibrated acceleration measurement range, and an auxiliary digital accelerometer channel with up to ±260m/s2 dynamic range. The SCH16T-K01 gyroscope offers extensive self-diagnostic features and angular rate and acceleration low pass filters ranging from 13Hz to 370Hz cut-off rate. 

Applications for SCH16T-K01 include inertial navigation and positioning, machine control and guidance, dynamic inclination, robotic control, and unmanned aerial vehicles (UAVs).

To learn more, visit https://www.mouser.com/new/murata/murata-sch16t-k01-gyroscopes/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Murata Electronics

2026 - Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764