Azoteq IQS7221E ProxFusion Sensor, Now at Mouser Electronics, Enables Integrated UI Applications

New Product Press Brief

Connect With Us


May 22, 2024 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the IQS7221E ProxFusion® sensor IC from Azoteq.

The Azoteq IQS7221E ProxFusion sensor is a fusion device with an on-axis orientation designed for rotation and angle sensing applications. This sensor IC includes a ProxFusion channel for integrated UI applications, enabling proximity and touch sensing. Two dedicated quadrature outputs make the product a drop-in replacement for mechanical and optical rotary encoders, and the virtual freewheel UI allows more intuitive scrolling. The IQS7221E sensor IC operates from a 2V to 3.5V voltage range. This sensor IC is available in WLCSP18 (1.62mm x 1.62mm x 0.5mm) and QFN20 (3mm x 3mm x 0.5mm) packages.

Typical applications for the IQS7221E include scroll wheels for computer peripherals, adjustment and control knobs, and motor encoders.

To learn more, visit https://www.mouser.com/new/azoteq/azoteq-iqs7221e-proxfusion-ic/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Azoteq

2026 - Azoteq is the world leader in capacitive proximity and touch solutions for next generation user interfaces. The ProxSense® capacitive sensors are the most sensitive and robust proximity and touch controllers available for use in touch keys, touch keypads, metal touch panels, non-ITO LCD screens, single layer ITO touch screens and 3D touch screens. The combination of proximity and touch enables new applications such as proximity wake up, backlight illumination and air gestures. Azoteq's ProxSense® provides the next evolution in user interfaces for consumer, medical, industrial and automotive applications.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764