Electronic Components
Stay ahead of the storm
Industrial Automation
Industrial Automation at your fingertips
In power electronics, designs rarely fail in simulation; they fail in the field. Engineers can validate efficiency, thermal margins, and transient response long before hardware is built. Yet real-world stresses, such as vibration, board flex, and thermal cycling, often reveal weaknesses that models never predict. This is especially true in industrial and energy systems where reliability is non-negotiable.
This week’s New Tech Tuesdays explores how stacked ceramic capacitor architectures help power designs maintain high-frequency performance while improving resistance to mechanical and thermal stress in harsh operating environments.
Multilayer ceramic capacitors (MLCCs) are a staple of modern power electronics thanks to their compact size and excellent high-frequency characteristics. However, conventional surface-mount MLCCs are rigid components soldered directly to rigid printed circuit boards (PCBs). When boards bend during assembly, installation, or operation, mechanical stress is transferred directly into the brittle ceramic dielectric.
This flex cracking is a significant post-assembly failure mechanism for MLCCs. These cracks may not cause immediate failure, but over time, they can progress from open circuits to short circuits, an especially dangerous condition on power rails.
Stacked ceramic capacitor architectures address these challenges by altering the mechanical coupling between the ceramic capacitor body and the PCB. Instead of mounting a single large ceramic body directly to the board, stacked designs combine multiple ceramic elements into a single assembly that connects via metal lead frames.
The lead frame provides a compliant mechanical interface that absorbs bending and thermal expansion, preventing stress from being transmitted to the ceramic layers. At the same time, stacking multiple elements allows designers to achieve higher capacitance values within the same mounting area, improving power density without increasing footprint.
Mechanical robustness alone is not enough for modern power systems. As switching frequencies increase to improve efficiency and transient response, the parasitic characteristics of capacitors become dominant design constraints.
Low equivalent series resistance (ESR) minimizes ripple losses and self-heating, while low equivalent series inductance (ESL) helps reduce voltage ringing and electromagnetic interference. Stacked ceramic constructions retain the low-parasitic behavior of ceramic capacitors while delivering the capacitance levels required for high-frequency power stages.
Applications such as downhole oil and gas electronics, industrial power supplies, and EV charging infrastructure push components well beyond office-temperature assumptions. These systems experience sustained vibration, wide temperature swings, and long operating lifetimes with limited opportunities for maintenance.
In these environments, components that absorb mechanical stress help maintain insulation resistance and reduce the likelihood of latent failures that appear long after deployment. Stacked capacitor architectures are specifically intended to address these combined electrical and mechanical demands.
KYOCERA AVX KGP series stacked capacitors are specifically designed for high-frequency operations, including rectifier and converter stages. Manufactured from green materials free of lead and cadmium, this commercial-grade series offers an environmentally conscious solution for demanding designs.
The KGP Series uses metal lead frames to absorb both heat and mechanical stress. This design provides excellent resistance to bending stress and suppresses weld cracking caused by thermal stress. Additionally, the KGP series capacitors feature low ESR and ESL, making them ideal for restraining noise in high-voltage coupling, DC-DC converters, and downhole applications.
The relentless push for higher power density and reliability in harsh environments means standard passive components are often no longer sufficient. Whether facing the extreme temperatures of downhole drilling or the rigorous demands of industrial power supplies, selecting the right component architecture is vital. Stacked capacitors with metal lead frames offer a proven path to achieving high capacitance, low parasitics, and exceptional mechanical resilience in your next-generation designs.
Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.