Electronic Components
Stay ahead of the storm
Industrial Automation
Industrial Automation at your fingertips
Embedded vision systems are evolving quickly, and with that evolution comes a shift in how designers approach system architecture. Cameras are now part of complex pipelines that include multiple sensors, interface bridges, real-time preprocessing, and edge artificial intelligence (AI) inference. As these elements converge, designers deliver more capability with smaller form factors and tighter power budgets.
Low-power field-programmable gate arrays (FPGAs) are emerging as efficient aggregation points for camera inputs and sensor data. They can bridge diverse interfaces, manage data flows, and perform early-stage processing without the overhead and latency of a full system-on-chip (SoC).
In this week’s New Tech Tuesdays, we explore how low-power FPGAs are reshaping embedded vision architectures, why they are gaining traction, and what designers can expect as edge systems continue to evolve.
The growth of embedded vision is driven by demand for intelligent endpoints, from smart cameras and industrial inspection systems to human-machine interfaces (HMIs). As more processing moves to the edge, sending raw video streams to the cloud becomes less practical because of latency, bandwidth, and privacy concerns.
At the same time, sensor ecosystems have become more fragmented, requiring designers to support Mobile Industry Processor Interface Camera Serial Interface 2® (MIPI CSI-2), Universal Serial Bus (USB), low-voltage differential signaling (LVDS), and other standards within a single system. Traditionally, bridging these interfaces required multiple chips or a large SoC, increasing power consumption and design complexity.
Low-power FPGAs address this challenge by serving as flexible glue logic and preprocessing engines. Unlike fixed-function application-specific integrated circuits (ASICs) or high-power SoCs, FPGAs enable designers to customize data paths and adapt to evolving requirements without redesigning hardware. They can manage multiple input streams, synchronize sensors, and perform tasks such as image scaling or filtering while maintaining deterministic latency and low power consumption. As edge AI moves inference closer to the device, FPGA-based aggregation is bringing control and preprocessing closer to the sensor layer.
As embedded vision evolves, the role of low-power FPGAs is expanding.
One trend is tighter integration with AI accelerators. FPGAs can serve as front-end processors that condition and route data efficiently into neural processing units (NPUs) or microcontrollers, reducing downstream workloads by sending selected, preprocessed data to the inference stage.
Power efficiency will also remain critical for always-on applications such as smart cameras, gesture recognition systems, and industrial monitoring devices. These use cases require architectures that remain responsive while minimizing standby and active power draw.
Another key direction is modularity and rapid prototyping. Designers need platforms that expose camera interfaces, support debugging, and allow quick iteration. System-on-module (SoM) platforms are enabling this shift by providing pre-integrated hardware blocks that accelerate development for smart endpoints and vision appliances.
Finally, scalability will continue to shape adoption. Designers need solutions that can evolve with their applications—from simple sensor aggregation to more advanced preprocessing—without requiring a complete system redesign.
For developers building low-power embedded vision systems, the Lattice Semiconductor CrossLinkU-NX SoM board offers a flexible and efficient platform for rapid prototyping and deployment. Built around Lattice’s low-power FPGA architecture, this SoM simplifies interface-heavy designs while maintaining tight power budgets. Its low-power FPGA enables designers to aggregate and manage multiple image streams without relying on a higher-power SoC, providing efficient data routing with predictable latency and low energy consumption.
The platform also supports common vision and connectivity interfaces, making it easier to bridge disparate sensor standards within the same design. This is particularly valuable in applications that combine multiple cameras or require compatibility across evolving interface ecosystems. Combined with integrated memory and high-speed input/output (I/O), the SoM can efficiently buffer and transfer preprocessing image data in real time, helping maintain throughput in multi-sensor environments.
Embedded vision has evolved beyond image capture to encompass the management of complex, interface-rich data pipelines at the edge. Low-power FPGAs serve as efficient aggregation and preprocessing hubs, giving designers the flexibility to build adaptable systems without sacrificing power or performance.
As edge devices continue to demand more intelligence in smaller footprints, these programmable FPGA-based solutions will play a central role in shaping the future of vision-enabled systems.
This blog was generated with assistance from Copilot for Microsoft 365.
Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.