Electronic Components
Stay ahead of the storm
Industrial Automation
Industrial Automation at your fingertips
Security consultants have long advocated “layers of security” for both physical and data systems. The strategy still applies when you are protecting the remote IoT and IIoT devices that are outside of your immediate control. In Part 1 of this series, we looked at protecting the MCU and boot process. In Part 2, we’ll look at protecting data and physical devices.
A determined attacker with much to gain from a hack will gladly disassemble even the most rugged device to find its vulnerabilities. Shipping production hardware with debug interfaces is a great way to make the hacker’s lives easier. It is well within the resources of hackers to purchase JTAG or SWD probes to read and write RAM, or re-flash on-chip memory. Peripheral TPM chips generally use an I2C or SPI interface directly to the MCU to prevent easy bus snooping, but are still vulnerable. The TPM hardware is delivered with a pre-programmed key that is never exposed to the rest of the system, and additional keys are typically derived from the factory-installed key, and never leave the module itself.
Eliminating debug interfaces provides an additional deterrent to malicious tampering.
It may be impractical to keep an eye on your sensing devices 24/7, particularly if you have deployed thousands of them. For this reason, it makes sense for your devices to keep an eye on themselves, and let you know if something undesirable happens.
Desktop computers have included intrusion detection switches for years that are capable of reporting when the enclosure is opened, but software to actually take action on such an event is relatively rare. Cover open alarms are more common in a server environment where out of band management software is much more widely used.
The principle is easily extended to IoT devices, where reporting the open/closed state of a switch is fairly trivial. Adding software to send an immediate alarm when the enclosure is opened provides a minimal degree of assurance that the device has not been tampered with. At the very least, the operations team that monitors the alarm can disregard data received from the sensor that was interfered with.
Up next in Part 3, we’ll look at protecting the network.