Electronic Components
Stay ahead of the storm
Industrial Automation
Industrial Automation at your fingertips
(Source: NOORULHASSAN/stock.adobe.com; generated with AI)
The industrial automation landscape is defined by deterministic control logic and the increasing data-intensiveness of digital transformation. To support these modern infrastructure needs, various controller architectures are used, such as programmable logic controllers (PLCs), programmable automation controllers (PACs), and industrial PCs.
However, as technology advances, the boundaries between these architectures have blurred. This creates a gray zone in which industrial controller selection depends more on the specific engineering constraints of the deployment. This blog does not aim to declare the best controller for industrial automation infrastructure, but rather to provide a decision framework guided by engineering requirements and trade-offs.
The execution model is at the core of an industrial automation system, controlling how processors interact with external physical triggers. The choice among scan-based, task-based, and event-driven models will determine the degree of determinism and their resilience to timing drift.
PLCs operate on a scan-based execution model: They scan the input, execute the program, and update the output. This model provides cyclical determinism, ensuring that each logic instruction is executed exactly once per cycle and that input and output (I/O) states remain consistent throughout execution.
The main advantage of the scan-based execution model is its predictability. For instance, a control engineer can calculate the exact maximum response time for the system. However, a limitation is that the logic execution is tied to the slowest part of the cycle. If communication tasks are not isolated or prioritized appropriately, they can extend the effective scan time and affect control responsiveness.
PACs and industrial PCs are moving away from simple scanning to a task-based or event-driven execution model. In these systems, the logic is organized into tasks with assigned priorities and execution intervals. The operating system (OS) scheduling algorithm handles preemption to allow high-priority tasks to interrupt their lower-priority counterparts.
Even the control application code is executed only in response to a specific trigger, such as a hardware interrupt or a software exception. These approaches optimize computation efficiency by sampling inputs only when necessary. However, these models increase the risk of unpredictable latency if multiple events occur simultaneously.
The OS controls the execution behavior of industrial controllers. PLCs are designed with real-time OS (RTOS) or bare-metal control loops, each optimized for industrial tasks. The firmware minimizes interference from non-control programs, resulting in high reliability for I/O scanning and logic execution.
PACs typically use an RTOS or a real-time execution layer on a general-purpose OS. For instance, a PAC may run a real-time Linux kernel, or a specialized OS that can preempt tasks reliably. Industrial PCs, on the other hand, run general-purpose OSs that are not designed to be real time. However, modern industrial PC control software installs a real-time extension that enables cyclical execution with higher priority than the general-purpose OS.
The most crucial aspect of any industrial automation infrastructure is the control system.
Motion control demands deterministic, high-frequency loop updates (often in the sub-millisecond range) and precise synchronization between axes. Traditional PLCs were not designed for multi-axis motion, and implementing complex motion required either adding separate motion controller modules or using smart drives. This led to fragmentation that was hard to maintain.
Modern PACs and advanced PLCs address this issue by integrating motion-control capabilities into the controller itself. A PAC generates multi-axis trajectories and coordinates axes in real time using standard networking interfaces, such as EtherCAT or SERCOS, to synchronize drives.
On the other hand, a typical industrial PC running Windows would struggle to ensure, for example, a consistent 1kHz update rate to eight servo axes. A non-real-time OS may experience occasional delays measuring tens-of-milliseconds due to scheduling, which is unsuitable in motion control. This constraint is why industrial PCs used for complex motion control are invariably equipped with real-time extensions or specialized motion hardware.
Industrial PCs with proper real-time setup are ideal for motion applications that demand intensive computation or data processing. For instance, a robotic cell that integrates real-time control with machine vision or artificial intelligence (AI) path optimization. A PLC or PAC might not have the computational power to handle vision processing or AI inference, whereas an industrial PC can handle all of it on a single platform.
When selecting a control architecture, engineers should systematically evaluate the application requirements. A decision framework can be outlined as follows:
System engineers must document the project’s key requirements, including the number of I/O points, required logic scan/update rates, motion-control needs, data-handling requirements, integration points, uptime requirements, environmental conditions, and any safety certifications. The requirement analysis should make clear which factors—such as speed, volume, complexity, and reliability—are most crucial.
It is important to understand the project’s complexity and the controller capabilities required to perform the job. For a simpler application, a PLC will meet the requirements at a lower cost and complexity. But if the application requires a complex architecture with multiple I/Os, many axes, and high data throughput, then it likely requires an advanced PAC- or IPC-based solution.
Beyond the initial hardware cost, engineers must also account for software licensing, engineering development time, training, and long-term maintenance. For example, the hardware cost of a PLC may be higher per I/O, but the engineering time to implement and maintain might be lower. For large, complex systems, the scalability of an industrial PC or PAC can be an advantage when factoring in the ability to consolidate functions.
Engineers must consider the expected life cycle and expansion of any automation application. If the system is expected to grow or require hardware upgrades, choosing a scalable platform is important. But when the project’s scope is fixed and unlikely to grow, a simpler PLC might be enough to avoid unnecessary complexity.
With modern industrial infrastructure requiring many varied automation demands, there is no one-size-fits-all industrial controller. The architectural choice should be driven by the project’s specific constraints and goals. An engineer’s task is to balance the trade-offs and combine platforms to create an optimal solution. By following a systematic evaluation, one can choose an architecture that is fit for purpose.
In the next installation of this PLC blog series, we take a closer look at the selection criteria driving control system decisions.
Abhishek Jadhav received his M.S. in Electrical and Computer Engineering and started his career as a technical writer. He has over five years’ experience working as a freelance technical writer, with key interests in power electronics and embedded systems. His work has appeared in EE Times, embedded.com, and Power Electronics News, among others.