Mouser Electronics - Electronic Components Distributor
 
Bulgaria - Flag Bulgaria

Please confirm your currency selection:

Euros
Incoterms:DDP
Incoterms: DDP (Duty and customs fees paid by Mouser).
Free shipping on most orders over 75 € (EUR).
All payment options available

US Dollars
Incoterms:DDP
Incoterms: DDP (Duty and customs fees paid by Mouser).
Free shipping on most orders over $90 (USD).
All payment options available

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


New Tech Tuesdays: Radiation-Hard GaN RF Advances LEO Satellite Connectivity Performance Darshan Mulki

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

The “New Space” era is no longer a concept but a bustling reality, dominated by massive low Earth orbit (LEO) satellite constellations. These constellations are the backbone of the integrated 5G and nascent 6G networks, promising to bridge the digital divide by delivering high-speed, low-latency connectivity to the most remote corners of the globe. However, the hostile environment of space remains a formidable barrier. To survive in such harsh conditions and deliver reliable performance, the radio frequency (RF) systems driving these connections rely on advanced materials like gallium nitride (GaN) and robust power management solutions.

This week’s New Tech Tuesdays explores the critical intersection of radiation-hardened electronics and next-generation connectivity by demonstrating how LEO constellations leverage GaN-based RF amplifiers to maintain vital links while withstanding cosmic radiation.

GaN and LEO Connectivity

Integrating LEO satellites with terrestrial networks is essential for meeting the “connecting the unconnected” goal of 5G and beyond.[1] Unlike geostationary (GEO) satellites, LEO constellations operate at lower altitudes of 300km to 2000km, which significantly reduces latency, a key performance indicator for vertical domains such as the Industrial Internet of Things (IIoT), remote eHealth monitoring, and intelligent vehicular networks.[2] However, to achieve the necessary data throughput and connectivity density, these satellites require high-performance RF systems capable of handling high power and wide bandwidths. This is where GaN technology becomes indispensable.

Compared to traditional gallium arsenide (GaAs) or silicon solutions, GaN offers superior power density and efficiency. According to recent studies, GaN’s high electron mobility facilitates rapid charge transport, which significantly reduces switching and conduction losses—a prerequisite for high-frequency operations in power-constrained satellite systems.[3] It also enables solid-state power amplifiers (SSPAs) that are smaller, lighter, and more efficient, which are critical factors for satellites’ weight and power budget constraints.

Furthermore, GaN boasts a wide bandgap of approximately 3.4eV and high bond strength, granting it intrinsic resistance to displacement damage and ionizing radiation. This capability allows GaN devices to operate reliably under the extreme thermal fluctuations and high-energy particle bombardment that are characteristic of the orbital environment. Research highlights that this resilience allows GaN to maintain stable carrier mobility and low-leakage currents, even when subjected to the extreme temperature cycles inherent to LEO missions, ensuring consistent signal integrity without heavy thermal shielding.[4]

While GaN RF power amplifiers handle transmission, the sophisticated digital logic—including field-programmable gate arrays (FPGAs) and application-specific integrated circuits (ASICs)—controlling these systems requires precise, clean, and radiation-hardened power. In the “New Space” paradigm, components must balance cost-effectiveness with radiation tolerance. As a result, the industry is moving towards plastic-packaged, radiation-hardened-by-design solutions that meet the typical three- to five-year lifespan requirements of LEO missions.

The Newest Products for Your Newest Designs®

To support the high power demands of LEO satellite electronics, STMicroelectronics has introduced the STEVAL-LEOPOL1V1 evaluation board (Figure 1). This board is designed to evaluate the LEOPOL1, a radiation-hardened 5A monolithic synchronous step-down regulator. The STEVAL-LEOPOL1V1 and LEOPOL1 chip are designed for LEO altitudes, offering a total ionizing dose (TID) immunity of 50 krad(Si). Additionally, the LEOPOL1 is single-event latch-up (SEL)-free up to 62MeV.cm2/mg, ensuring reliability against cosmic rays.

Figure 1: The STMicroelectronics STEVAL-LEOPOL1V1 evaluation board was developed and optimized for a typical LEOPOL1 application. (Source: Mouser Electronics)

The STEVAL-LEOPOL1V1 creates a compact, efficient power supply solution optimized for the harsh conditions of space. The board features a specific design to evaluate the LEOPOL1 regulator, which converts input voltages from 3V to 12V down to a regulated output. This feature makes it ideal for powering the FPGAs, microcontrollers, and ASICs that manage satellite RF communications and data processing. The board also utilizes a PowerSO-36 package, aligning with the “New Space” requirement for cost-effective components that deliver space-grade performance.

Tuesday’s Takeaway

As LEO constellations reshape vertical industries from agriculture to energy by providing global 5G coverage, the hardware orbiting above us must be as resilient as it is powerful. The synergy between GaN-based RF systems and robust power management empowers LEO constellations to maintain the vital 5G and 6G links the modern world depends on.

   

Sources

[1] https://ctu.ieee.org/
[2] https://doi.org/10.1109/MCOM.001.2001081
[3] https://doi.org/10.3390/mi16121421
[4] https://doi.org/10.3390/mi16121421



« Back


Darshan Mulki is a Product Content Specialist at Mouser Electronics. He graduated with a Bachelor of Engineering (BE) degree in Electronics and Communication(ECE) and has over ten years of experience writing about technology. Darshan has a passion for exploring the latest developments in technology and uses his penchant for creating engaging and informative content to make complex technological concepts accessible to readers, providing valuable insights into how technology impacts our daily lives. Darshan draws inspiration from the transformative effect that technology has had on everyone in the world and constantly explores the implications of emerging technologies on society and the future of our planet.


All Authors

Show More Show More
View Blogs by Date

Archives