How Tiny Hall Switches Save Space in Portable Devices Diodes Incorporated

(Source: Diodes Incorporated)

The electronics industry possesses a never-ending drive for lower power consumption and more compact devices. It is most obvious in battery-powered consumer products, such as wearables, smartphones, and wireless earbuds. The demands for smaller and power-efficient solutions hold true almost everywhere—across home appliances, industrial applications, data centers, and more.

Every component in a system design needs to be analyzed in terms of these two objectives: “can it be smaller,” and “can it use less power.” At the same time, we cannot compromise on performance, reliability, and cost. For switches in portable, battery-powered devices, the solution to meeting these challenges is often to use a Hall-effect sensor—yearly sales of over $1.5 billion[1] show how popular this type of component is.

These sensors are based on the Hall effect: When a current-carrying conductor is placed into a magnetic field, a voltage will be generated perpendicular to both the current and the field. This voltage is proportional to the strength of the magnetic field. Hall sensors are ideal for use in many types of switches, where they can simply detect the presence or absence of a small permanent magnet. They are often used in proximity sensing applications, such as detecting whether a laptop’s lid is open or closed. Since the switches are contactless, they are reliable and have a long operating life.

To meet the demand for small, power-efficient switches, Diodes Incorporated launched the AH138x and AH139x. This is a family of micropower, push-pull, unipolar Hall switches that are ideal for portable, battery-powered devices.

The two switches differ in the outputs provided. First, the AH139x series has two outputs: one responds to a North pole, the other responds to a South pole. The AH138x series has a single output, which responds to a South pole.

These devices have a wide input voltage range of 1.6V to 5.5V. As a result, they can be powered directly from a battery, thus eliminating the cost and board space demands of power conversion. They only require an ultra-low 1.6μA (typical) average supply current over the full voltage range, and this drops to only 1.1µA at 1.85V. This means that power consumption is minimized, helping extend battery life.

A pull-up resistor is unnecessary as the AH138x and AH139x have an internal push-pull output structure to reduce external component count. This makes the design simpler and smaller, further saving board space.

All switches in this family are provided in compact DFN1010-4 and DFN1410-4 packages, and the AH1381, AH1382, and AH1383 versions are additionally available in SOT23 packages. They have high electrostatic (ESD) protection to improve their robustness and reliability.

Overall, the AH138x and AH139x provide small, simple, and flexible contactless switch solutions for portable, battery-powered applications.

Author

Charles Kuo, Product Line Manager, Diodes Incorporated
Charles is a Product Line Manager at Diodes Incorporated, possessing extensive engineering expertise in power management, and magnetic sensor technologies. With a BS in Electronic Engineering and an MBA, he brings a strong technical foundation complemented by strategic business acumen. Prior to Diodes, Charles contributed significantly to the semiconductor industry through roles at NXP Semiconductors and Texas Instruments.

The blog "How Tiny Hall Switches Save Space in Portable Devices" was first published on https://www.diodes.com/ and is reposted here with permission.

 

 

Sources

[1] Hall Effect Sensor Market Size, Share, Opportunities, And Trends By Type (Hall Switch, Linear Hall Sensors), By End-User (Industrial, Automotive, Electrical & Electronics, Others), And By Geography - Forecasts From 2023 To 2028, July 2023. https://www.knowledge-sourcing.com/report/hall-effect-sensor-market.



« Back


Diodes IncorporatedDiodes Incorporated delivers high-quality semiconductor products to the world’s leading companies in the automotive, industrial, computing, consumer electronics, and communications markets. Diodes Incorporated leverages its expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. The company's broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 32 sites, including engineering, testing, manufacturing, and customer service, enables Diodes Incorporated to be a premier provider for high-volume, high-growth markets.


All Authors

Show More Show More
View Blogs by Date

Archives