IoT Sensor Node Block Diagram
The Internet of Things (IoT) is about interconnecting embedded systems, bringing together two evolving
technologies: wireless connectivity and sensors. These connected embedded systems are independent
microcontroller-based computers that use sensors to collect data. These IoT systems are networked together
usually by a wireless protocol such as WiFi, Bluetooth, 802.11.4, or a custom communication system. The
networking protocol is selected based on the distribution of nodes and the amount of data to be collected.
This data is sent over the network to the main hub or computer. This main computer collects and analyzes the
data, storing it in memory and even making system decisions based on the results of the analysis.
Crucial to modern IoT nodes is the need for security with some form of data encryption, the most common being
AES256. This security is critical for helping the microcontroller perform a secure boot, insuring that the
core is running the code is meant to run. Encryption security is also used to encrypt the data transmitted
over the network, insuring that it is viewed only by those systems authorized to receive the data.
IoT Sensor Node Block Diagram
View Product List
This design is for reference only. The design, as well as the products suggested, has not been tested
for compatibility or interoperability.